STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Blank check with STM32_Programmer_CLI.exe

I make a blankcheck of a device with this command:STM32_Programmer_CLI.exe" "-c port=swd UR -blankcheck"This command returns ERRORLEVEL == 0 if the device is blank, but also if the devices is programmed.How can I, from the command line, find out if a...

UW by Associate
  • 1549 Views
  • 2 replies
  • 1 kudos

Resolved! CubeProgrammer API downlaodFile error

Hey there,I am using the CubeProgrammer API (2.17.0) to flash a STM32U545 MCU over USB DFU with a new firmware.When doing so a write error occurs (downlaodFile(...) returns CUBEPROGRAMMER_ERROR_WRITE_MEM (-10)) when flashing a new hex file (when usin...

WhoIsJohnGalt_0-1728972907764.png

Resolved! Can't download the program!! :(

Hello, I want to download the program, STM32CubeProgrammer.Before log in, download tap was visible and connectable.However, After log in, download tap continues to load...I've been waiting a long time, but it doesn't stop!!! :(I also cleaned my cache...

imege.PNG
inkong by Associate II
  • 4139 Views
  • 4 replies
  • 3 kudos

please improve STMProg

Please Never use a popup any where in the app its extremely annoying, use a window I propse you call it "Console" or "LOG " .. oh what do you know you already have one!!!.. so please stop with the popups... also remove the Refresh button Let Connect ...

NCD by Associate II
  • 5418 Views
  • 10 replies
  • 0 kudos

Using st link v3 to program over CAN

Good day,I am attempting to program an STM32L5 MCU using an ST Link V3 over FDCAN. I am aware that on the breakout board for the ST Link V3 there is connector CN5 which has CAN RX and TX. On the microcontroller I have a CAN transceiver installed on p...

Eben_0-1717506462665.png
Eben by Associate II
  • 3566 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.