STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Empty lines added by --safelib command into .hex

Starting from V2.13 the STM32CubeProgrammer_CLI adds strange empty lines into the .hex file when adding CRCs using the --safelib command.Example:...:20F9C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF47:20F9E000FFFFFFFFFFFFFFFFFF...

DFlam.1 by Associate
  • 1048 Views
  • 2 replies
  • 0 kudos

Resolved! STM32N6 Flash Memory Protection

I'm trying to flash an an NUCLEO-N657X0-Q board with the STM32N6 using STM32CubeProgrammer v2.20.0. I have two NUCLEO-N657X0-Q boards here: One of them flashes just fine, the other one refuses to work. Both boards are in development mode (BOOT jumper...

Jeija_0-1761678820914.png
Jeija by Associate
  • 924 Views
  • 2 replies
  • 0 kudos

STM32CubeProgrammer proper jlink error handling

It would be great if the STM32CubeProgrammer would do proper error handling for J-Link debug probes instead of crashing.Issue:Every times I try to the connect to a STM32 target that is not powered, or not properly connected the GUI pops up three erro...

Tom_pm by Associate III
  • 819 Views
  • 1 replies
  • 1 kudos

Resolved! NUCLEO-N657X0-Q: Unable to erase flash

Hi,I've recently been trying to get an LRUN application up and running on the NUCLEO-N657X0-Q board. Similar to the posts in https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32n6570-dk-unable-to-erase-external-flash/td-p/757897, I cannot acces...

michaelg643_1-1755967138338.png michaelg643_0-1755966866504.png

STM32CubeProgrammer v2.21 released

We are pleased to announce that STM32CubeProgrammer 2.21 is available What is new in 2.21: • Support for the STM32WL3Rxx microcontrollers:         – Internal memory programming        – Option byte and OTP programming         – PKCS#11        – Firmw...

STM32CubeProgrammer erase fails under Linux

I noticed that the V 2.20 STM32CubeProgrammer erase function doesn't work under Pop_OS!, a Linux distribution.  It does however work on Windows 10.  I don't think this is a logic failure within the STM32CubeProgrammer but some weird interaction with ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.