STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer gives error: "No STM32 target found!"

I have a custom board with one STM32H743ZIT6 (“Control MCU�?) and six STM32H7V43VIT6 MCUs. The idea, eventually, is for the Control MCU to reset the six slave MCUs.Right now, after an initial flashing of the slaves with a “bring up�? blinky program t...

APagl by Associate III
  • 2224 Views
  • 2 replies
  • 0 kudos

STM32CubeProgrammer fails to program STM32L0s MCU when the size of the file to program is not a multiple of 8.

Hi,I am experiencing a problem with STM32CubeProgrammer: it fails to program STM32L0s MCU when the size of the file to program is not a multiple of 8.In the attached zip file, there are 2 .bin files containing 16 bytes of zeros (working.bin), and 20 ...

olivier by Associate III
  • 4321 Views
  • 8 replies
  • 0 kudos

How to update the FW by CubeProgrammer via USART?

I want to update the FW to H7 MCU via its USART by embedded bootloader. It seems need to control the BOOT0 pin and nRST pin when the MCU is in normal running. By CubeProg tool, how to control above 2 pins by PC? Usually, I will build a USB to UART br...

JZou.2 by Associate II
  • 2962 Views
  • 8 replies
  • 0 kudos

Resolved! STM32CubeProgrammer SREC behaviour

Hi,I recently stumbled on a issue.For a project we developed a bootloader which checks the programs CRC if it matches and halts if not. The CRC is calculated after linking and is placed in front of the application.I found out that there is a differen...

Mvan .31 by Associate II
  • 3259 Views
  • 2 replies
  • 0 kudos

STM32CubeProgrammer 2.4.0 released

New features • Added the support of the graphic user interface (GUI) for the firmware upgrade service (FUS) and stack upgrade for the entire STM32WB Series • Support of HSM V2 on all STM32 microcontrollers and microprocessors supporting SFI/SSP Fixed...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.