2020-08-07 11:23 AM
I have a custom board with one STM32H743ZIT6 (“Control MCU�?) and six STM32H7V43VIT6 MCUs. The idea, eventually, is for the Control MCU to reset the six slave MCUs.
Right now, after an initial flashing of the slaves with a “bring up�? blinky program they run after reset. However, I cannot now flash anything to them. For example, in SW4STM32 Workbench on my MacBookPro ….
With the debug cfg file with “Connect under reset�? or “Hardware reset�? or “Software system reset�?, I get STLINK_SWD_AP_WDATA_ERROR and auto_probe failed errors in the console.
So, I now have STM32CubeProgrammer installed, version 2.5.0. Besides it’s randomly crashing from time to time, when it behaves, I cannot connect to any of the slaves. CubeProgrammer gives the error: “Error: No STM32 target found!�?
BTW, each slave MCUhas a 10-pin JTAG connector properly wired up (3.3V from the board, GND, SWCLK, SWDIO, SWO, RST). I have done connectivity tests along the route from the ST-LINK/V2 module all the way to the 10-pin header connector.
After Googling around, I seem to get the impression that I should use CubeProgrammer to erase the MCU and reload with the debug pins configured (via, for example, CubeMX). However, since I constantly get the No STM32 target found upon trying to connect to the MCU, I seem to be stuck.
The slaves have their NRST pins pulled down with 10K (so that the Control MCU can reset them when needed).
I see things that suggest pulling RST high or BOOT0 high, but I’ve tried those while trying to connect via CubeProgrammer.
Questions:
Any way out of this Catch-22?
Thanks.
2020-08-07 12:11 PM
NRST is driven internally with an Open-Drain, you're supposed to pull-up, and NEVER drive the signal high with a push-pull on this or other parts of the circuit.
Pulling BOOT0 High allows the ROM loader to run, preventing errant user code running.
Does your code interfere with the JTAG/SWD pins, disable the interface, or go into low power modes?
Getting the SMPS/VOS settings wrong can make it very difficult to connect to the core.
If you can't get in via JTAG/SWD, you could try other ROM loader methods via USART
2020-08-07 12:13 PM
If these are brand new chips, there should be no need to erase/configure anything before you can connect with SWD. Try a lower SWD clock speed.
The SWCLK/SWDIO lines for each header are only connected to a single chip, right? Not the same net for all chips?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.