STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! NEWBIE Unable To Debug Or Run Simple Blinky Project

Hi everyone, I recently got a Nucleo board (STM32L476RG) to introduce myself to the stm32 mcu and I've installed the stm32cubeide alongside it. I've been trying to run a simple blinky project for the past hour but I keep getting this message, "Waitin...

0693W000003Q2BPQA0.jpg
TNguy.18 by Associate II
  • 2675 Views
  • 4 replies
  • 0 kudos

STM32H7B3i-DK Error: No STM32 target found

The STMCubeProgrammer would no longer connect to my target. I was able to create a simple test program with Keil toolchain and step through the code and suddenly I noticed that the board stopped responding.I then tried connecting to the board with ST...

onio by Senior
  • 4310 Views
  • 9 replies
  • 2 kudos

RDP Level 1->0: Can ANYTHING survive ??

I am using STMCubeProgrammer in USB DFU mode to change from RDP Level 1 to 0 (using command line -rdu option). This nukes (mass erases) all flash and all "backup SRAM" (according to datasheet).My product has a couple of bytes of custom config data ...

Goof Ball by Associate III
  • 1590 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.