STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

I can't burn or debug a project on STM32 IDE

I'm working with Windows 10 and STM Ide version 1.5.1.I have a project made it with CubeMX.  I use FreeRTOS and some HAL libraries.I can compile correctly:arm-none-eabi-size  ST-2100.elf arm-none-eabi-objdump -h -S ST-2100.elf > "ST-2100.list"arm-non...

JRios by Associate II
  • 4320 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F030 Data mismatch error

Hi, I am facing up Error: Data mismatch found at address error. I have tried to decrease the frequency, also make a modification to the linker script. Also, I used OCD. But, no success. When I open a new project it uploads. Whenever I change somethin...

SWV Console Automated

Hi there,I've an issue when trying to automatize the SWV command with Jenkins. The issue is that when I run the command: STM32_Programmer_CLI -c port=SWD -swv freq=216 portnumber=0 it asks the user to press 'R' in order to start. Since Jenkins has no...

0693W000007ZqaKQAS.jpg
RCast.2 by Associate
  • 1794 Views
  • 3 replies
  • 1 kudos

Problem Erasing Chip Memory - Read Out Protection

Hello everyone!I work with a Nucleo board F446RE. One month ago i lended my board to one of my university collegue. After a while he gave me back my board, but i can't use it anymore. When I try to flash a program with STM32Cube IDE it gives me an er...

RHuzy.1 by Associate II
  • 3458 Views
  • 6 replies
  • 0 kudos

Resolved! SWD connection no longer working

Hello,On a STM32L4 design, we no longer have an SWD connection to the processor: using STM32CubeProgrammer reports ST-LINK SN : 39FF6A064243383912381057ST-LINK FW : V2J36S7Voltage : 3.26VSWD freq : 4000 KHzConnect mode: NormalReset mode : Software re...

RHaag.1 by Associate II
  • 6106 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.