2021-03-10 12:12 PM
I'm working with Windows 10 and STM Ide version 1.5.1.
I have a project made it with CubeMX. I use FreeRTOS and some HAL libraries.
I can compile correctly:
arm-none-eabi-size ST-2100.elf
arm-none-eabi-objdump -h -S ST-2100.elf > "ST-2100.list"
arm-none-eabi-objcopy -O binary ST-2100.elf "ST-2100.bin"
text data bss dec hex filename
46372 20 16416 62808 f558 ST-2100.elf
Finished building: default.size.stdout
Finished building: ST-2100.bin
Finished building: ST-2100.list
I could debug it before, but now, when I try to debug it, I get same response:
STMicroelectronics ST-LINK GDB server. Version 5.7.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.6.0-RC3
-------------------------------------------------------------------
ST-LINK SN : 066AFF485550755187253829
ST-LINK FW : V2J37M26
Board : NUCLEO-L053R8
Voltage : 3.25V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x442
Revision ID : Rev 1.0
Device name : STM32F09x/F030xC
Flash size : 256 KBytes
Device type : MCU
Device CPU : Cortex-M0
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a02004.srec
File : ST-LINK_GDB_server_a02004.srec
Size : 46396 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 22]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:02.267
Verifying ...
Error: Data mismatch found at address 0x08004064 (byte = 0x33 instead of 0x01)
Error: Download verification failed
Encountered Error when opening C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.5.0.202011040924\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
STM32_Programmer_CLI.exe exists on that path, its version is 2.7.0-RC1
more stuff, appears a message window with this text:
Error in final launch sequence:
Failed to execute MI command:
load C:\\ws-1.15\\ST-2100\\Debug\\ST-2100.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\ws-1.15\\ST-2100\\Debug\\ST-2100.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\ws-1.15\\ST-2100\\Debug\\ST-2100.elf
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation
This error isn't new for me, last year some times I got this error, my solution was made a new workspace, import my project and then worked fine, but today I can't do it fix with my "recipe".
I create a new workspace, then a a new project from zero with CubeMX or ST Ide, generate code and then debug without a modification of generated code, I get always same response.
I updated ST Cube IDE from 1.5.1 to 1.6 and the problem persists.
I don't know what can I do to solve it.
Why appears a double slash on path?:
=> load C:\\ws-1.15\\ST-2100\\Debug\\ST-2100.elf
How I can resolve this?
2021-03-10 12:21 PM
Update:
I use a STM32F091RC microcontroller and a nucleo L053 or ST Link V2 for programming, behaviour is the same.
2021-03-16 2:40 PM
This as a possible fix.
Today I tried programming the Nucleo G071RB with the X-NUCLEO_GFX01M1 LCD running the Demo program and got similar errors.
Since I usually buy my Dev board in pairs, the other G071RB worked first time.
These two boards are the same revision number, production date and even have serial numbers only 300 apart from each other.(Firmware version: V2J37M27)
2021-03-19 3:29 PM
Thanks for your answer. I'm so sorry, but I don't understand what is the solution.
Can you explain me with details, please?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.