STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32F030C8T6> connect with STLINKv2 & STCube Programmer..... I want to flash firmware using SWO port. Pin connections are TVCC(pin1), SWCLK(9), SWIO(7), STM32rst(15) GND(12).

 Error: No STM32 target found! This is the CONSTANT message I get from the STCUBE software. I can see reference voltage from my board but actually connecting to the chip is impossible  Error: No STM32 target found!,  Error: No STM32 target found!, Er...

AHolm.1 by Associate
  • 2230 Views
  • 2 replies
  • 0 kudos

No ST-LINK detected in STM32CubeProgrammer

Hi,I'm having some trouble with getting my (genuine) ST-LINK v2 detected in the STM32CubeProgrammer. The strange thing is, the STM32CubeIDE and also the firmware update utility detect the ST-LINK v2 without any issues. Already tried different USB por...

0693W000007ZGORQA4.png
HGreg.1 by Associate II
  • 2095 Views
  • 5 replies
  • 1 kudos

Flashing stm32h7b3-dk issue,

 I am trying to restore the demo file that came with this discovery kit. Erase all works but when I try to program it I get these errors after the erase is complete: 17:48:08 : Download in Progress: 17:48:11 : Error: failed to download Segment[9] 17:...

JWalt.1 by Associate II
  • 2168 Views
  • 4 replies
  • 0 kudos

Resolved! STM32 Programmer USB DFU fails using GUI

I can successfully program a STM32L082 over USB when using STM32_Programmer_CLI.exe but not using the GUI. I can see the device under USB but I get "Error: Data read failed" followed by "Warning: Connection to device 0x447 is lost" when clicking the...

EDavey by Associate
  • 2008 Views
  • 3 replies
  • 0 kudos

Resolved! Flashing bin from custom Start address

Good evening to you all electronics dark wizards.To the point:I am interested in flashing specific pages of stm32 chips because im locating some custom binary config files for my application.I found the option in my stm32cubeprogrammer v2.6.0 to defi...

0693W000007EgsVQAS.png 0693W000007Eh1IQAS.png 0693W000007Eh50QAC.png
Javier1 by Principal
  • 2552 Views
  • 2 replies
  • 0 kudos

Resolved! Not able to connect to NUCLEO-H755ZI-Q

Hi,I am developing some code for a display interface on a NUCLEO-H755ZI-Q, I debug some basic code and the STM32 seem to have crashed.Now I can not connect anymore to it, not even with the CubeProgrammer V2.5.Is there a way to recover the Nucleo boar...

Marco.D by Associate II
  • 4938 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.