STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer error message !

I use STM32CubeProgrammer, but i can't use STME2CubeProgreammerI try to connect it to board, but error message happen.below error message.07:02:43 : ST-LINK SN : 066DFF383337554E4312365507:02:43 : ST-LINK FW : V2J37M2707:02:43 : Board    : NUCLEO-G07...

MYu.1 by Associate II
  • 1187 Views
  • 1 replies
  • 0 kudos

Resolved! Error: failed to download Segment[0]

HI, ST​Im trying to fw update using MFC Tool, STM32_Programmer_CLI.exe.​first, i checked that the fw download operation was completed using Terminal.so, I makeed the mfc tool in the way the terminal works in the background and checked the fw download...

JPark.20 by Associate II
  • 3563 Views
  • 2 replies
  • 0 kudos

STM32CubeProgrammer 2.7.0 released

New features• Added the support for the STM32WB15xx microcontrollers in the STM32WB Series• Added the support for the microcontrollers with 64 Kbytes of Flash memory in the STM32G0 Series• Added HardFault Analyzer support• Added Register viewer suppo...

Flash NUCLEO-H743 with UART in CubeProgrammer

I have NUCLEO-H743 board. After I load the firmware with this pin configuration, the board began to give an error STLINK (PB4 is NJTRST). Initially, the board was flashed even with this configuration, but after Debugging it stopped. I was advised to ...

0693W000008yaFTQAY.png 0693W000008yaFOQAY.png
MZoto.1 by Associate
  • 1206 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.