2021-04-26 3:09 PM
I use STM32CubeProgrammer, but i can't use STME2CubeProgreammer
I try to connect it to board, but error message happen.
below error message.
07:02:43 : ST-LINK SN : 066DFF383337554E43123655
07:02:43 : ST-LINK FW : V2J37M27
07:02:43 : Board : NUCLEO-G070RB
07:02:43 : Voltage : 3.22V
07:02:43 : Error: No STM32 target found!
i already did frimware upgrrade
2021-04-26 3:18 PM
Assuming the connection is correct, I guess you didn't enable SWD.
If you didn't enable the SWD interface in the firmware, It will be disabled after booting, the programmer won't be able to connect unless you use nRST pin, or manually hold nRST low before clicking on Program, and then release.
The manual method requires some tries until getting the correct timming
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.