2021-04-20 8:19 PM
HI, ST
Im trying to fw update using MFC Tool, STM32_Programmer_CLI.exe.
first, i checked that the fw download operation was completed using Terminal.
so, I makeed the mfc tool in the way the terminal works in the background and checked the fw download works, but it doesn't work well.
this is the output on Debug message(using TRACE()):
[command : STM32_Programmer_CLI.exe -c port=usb1 -d C:\TEST\TEST.bin 0x08000000]
-------------------------------------------------------------------
STM32CubeProgrammer v2.5.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : STM32 BOOTLOADER
SN : 205530724352
FW version : 0x011a
Device ID : 0x0470
Device name : STM32L4Rxxx/STM32L4Sxxx
Flash size : 2 MBytes (default)
Device type : MCU
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: TEST.bin
File : TEST.bin
Size : 645823 Bytes
Address : 0x80000000
Erasing memory corresponding to segment 0:
Not flash Memory : No erase done
Download in Progress:
0%
Error: failed to download Segment[0]
Error: failed to download the File
---------------------------------------------------------------------------------------------------------------------------------------
it doesn't seem to be working from erasing memory before updating. (likewise, '--skipperase')
I appeciate any comment or suggestions
thanks you!!
Solved! Go to Solution.
2021-04-21 10:12 AM
Indeed, 0x80000000 is not flash memory (should it be 0x08000000 ?)
--pa
2021-04-21 10:12 AM
Indeed, 0x80000000 is not flash memory (should it be 0x08000000 ?)
--pa
2021-04-21 6:19 PM
yes! im fool!!!!!!!
thanks you Pavel!!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.