STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Program crash if MCU not powered

I wanted to connect to my STM32 MCU with STM32CubeProgrammer but forgot to power on the board. The programmers (I had 2 boards with 2 STLINK-v3MINIs connected) were detected but when I connected to one, STM32CubeProgrammer crashed. When powered every...

Arno1 by Senior
  • 841 Views
  • 0 replies
  • 1 kudos

AT25SF128A External Flash Loader

Hi, I used MT25QL128 flash memory in my project. This product was obsolute then, I decided to use AT12SF128 flash memory instead of MT25QL128 . Now, I use STM32 Cube Programmer and can not write external memory . Program give "memory edition verifica...

Nbaşa.1 by Associate II
  • 15233 Views
  • 15 replies
  • 0 kudos

Resolved! STM32Cube Programmer

Hi amazing forum.. I am wondering if there is a way to save as HEX file the memory read from the stm32 cube programmer.. I am asking this because I want to check that the bootloader that I am creating is exaclty writing what I expect ...Thanks a lot...

SGasp.1 by Senior
  • 7324 Views
  • 4 replies
  • 1 kudos

STM32CubeProgrammer 2.8.0

New features • Added the support for the STM32U575/585 microcontrollers • Added the support for SFI via the JTAG interface for the STM32U575/585 microcontrollers • Added the support for SFI via the bootloader interface (USB/UART/I2C/SPI) for the STM3...

Resolved! Quadspi image/font data stored wrongly

Board Name : stm32f7 seriesQUADSPI : N25Q128AI am stored imaged data in nor flash, data stored correctly in memory. After i am reset the controller or power on the controller, data will be resetExample :data : 0xD3005600Data stored first time p...

0693W00000FCADOQA5.png 0693W00000FCAEvQAP.png

How to erase external flash from CLI?

I would like to erase the external flash from terminal using STM32_Programmer_CLI.Using the command STM32_Programmer_CLI -c port=SWD freq=4000 mode=UR -el MX25LM51245G_STM32H735G-DK.stldr --erase alldoes not seem to erase the external flash.Giving th...

Arno1 by Senior
  • 1096 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.