2021-07-26 1:55 AM
New features
• Added the support for the STM32U575/585 microcontrollers
• Added the support for SFI via the JTAG interface for the STM32U575/585 microcontrollers
• Added the support for SFI via the bootloader interface (USB/UART/I2C/SPI) for the STM32U5 Series
• Added the new FUS-Operator support for the STM32WB1xxx microcontrollers
• Added the anti-rollback support for the STM32WB1xxx and STM32WB5xxx microcontrollers
• Added the support of FUS version display for the STM32WB1xxx and STM32WB5xxx microcontrollers
• Added the support for the Live Grid Update feature
• Added the support for the Blank check feature
• Added the support for the Memory/File and File/File compare features
• Added the support for the bootloader version display feature
• Added the support for the Fill memory feature
• Added the support for UART interface RTS/CTS signals
• Added the support for Connect while Watchdog enabled
Main issues fixed in STM32CubeProgrammer v2.8.0
2021-10-04 10:36 AM
STM32CubeProgrammer v2.8.0 remains seriously broken.
When running with OpenJDK 11 (Azul JDK), 2.8.0 silently fails when programming STM32L471 targets via UART (a subsequent verify shows the failure). This is 100% reproducible. I've been reporting serious flash programming bugs for these targets for nearly a year (since 2.5.0) (ref. case 00135468 and see also STM32CubeProgrammer is not able to successfully connect to or flash an STM32L471. This is a long-standing problem. I have no problem flashing other STM32L parts such as L051 and I have no problem flashing the L471 using an STLinkv2.)
Are there plans to fix STM32CubeProgrammer? Is there an alternate solution?
2021-10-16 12:21 PM
Installer for MacOS version cannot start at all. Even some hack to start, there is error to copy JRE. And no way to start the programmer at all. This problem exists for more than half year.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.