STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer cannot finish installing

I am trying to install STM32CubeProgrammer v2.8.0 on my Windows10 (Home x64) computer. I have updated my Java version to 8.301 (64-bit). However, installation process doesn't go further than Step 7 out of 8. There's no "Next" button or something, b...

RDermenci by Associate II
  • 1240 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H743 .bin file is enormous

Hi !I'm used to working with F4 and F7 devices, and I've always made '.bin' files to distribute the firmware upgrades, which can be flashed via a custom bootloader, directly on the board, from an SD card.With my current project however, on a STM32H74...

TGeof.2 by Associate II
  • 5638 Views
  • 8 replies
  • 0 kudos

Resolved! Meaning of "Value" Field in Option Bytes STM32

I am trying to understand the semantics of the "value" field in the option bytes in Cube Programmer. On my STM32G0 part, the PCROP1A_STRT and PCROP1A_END fields have "value" and "address" fields. What are valid inputs for the "value" field? Thanks!

0693W00000FBwiIQAT.jpg
RKher.1 by Associate III
  • 1260 Views
  • 1 replies
  • 0 kudos

STM32cubeProgrammer 2.8.0 download shutdown

hello, so i use STM32cubeprogrammer, so i want firmware but i cant use this program coz The program is forcibly terminated by connecting the device and pressing Download to upload the firmware file. I don't know why. Does anyone know why this is hap...

Mseon.1 by Associate
  • 1444 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 Programmer CLI hangs on parsing large file

I am trying to program an F4 with an external flash chip in mapped memory mode using the STM32_Programmer_CLI. I use the cli commandSTM32_Programmer_CLI.exe --connect port=SWD mode=UR reset=hwRst -halt --erase all --download <path_to_hex> -el <path>...

GDare.1 by Associate II
  • 7567 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.