STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer crashes when connecting to ST/Link

Hi: I've installed STM32CubeProgrammer and when connecting to the STLink debug programmer it worked ok. But now, it just crashes. I've tested three different probes, on two different computers.Both computers are running Linux (Arch Linux), kernel ver...

FDami.1 by Associate II
  • 1668 Views
  • 1 replies
  • 0 kudos

Resolved! DFUse does not detect my STM32 devices

Hello,I want to flash micropython in one of my stm32 devices. In order to flash micropython I need to put the stm32 board in DFU mode connecting the VDD pin to BOOT0.When I do this and I reboot the board, the behaviour of the board changes (the defau...

Hello there, After the application I developed with STM32G0B1VC exceeds 128KB, STM32CubeIde(v1.7.0) gives the following message.

Erasing memory corresponding to segment 0:Erasing internal memory sectors [0 64]Download in Progress:Error: failed to down In this case, I am erasing with STM32CubeProgrammer(v2.8.0). When I run it again with STM32CubeIde I get the following message ...

zekeriya by Associate II
  • 3753 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.