2022-05-29 7:41 PM
Hello everyone, I'm a beginner and want to try STM32 but there is a problem when installing STM32cube programming the message "CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program of check your java".
I use :
osx :10.9.5
java version "1.8.0_331"
Java(TM) SE Runtime Environment (build 1.8.0_331-b09)
Java HotSpot(TM) 64-Bit Server VM (build 25.331-b09, mixed mode).
Thanks everyone hope someone can tell how to solve it.
2022-06-15 1:33 PM
Hello @TKamp.1 and welcome to the Community :)
Run STM32CubeProgrammer using admin rights.
There is no need to install any Java SE Run Time Environment since version 2.6.0.
The STM32CubeProgrammer runs with a bundled JRE available within the downloaded package and no longer with the one installed on your machine.
Please follow the UM2237 which describes the requirements and procedures to install the STM32CubeProgrammer software tool.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.