STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32U5 HAL_FLASH_Unlock() fails

Hello everybody!Our company's QA reported some devices with STM32U585VIT6 CPU in a state when write to Flash became impossible.As a developer, I tried to reproduce this and after some experiments got stuck in a strange state when HAL_FLASH_Unlock ret...

micklecat by Associate II
  • 5175 Views
  • 4 replies
  • 0 kudos

Why do I get the error: 'Error: Data read failed'

I have an STM32F030K6T6, I 'm using STM32CubeProgrammer with ST-Link V2.I click 'connect' and I get this error:'Error: Data read failed'It gets connected to the MCU, reads correctly it's ID.I have checked all related connections: SWCLK, SWDIO, RST, 3...

STM32CubeProgrammer 2.12.0 released

We are pleased to announce you that the official release of STM32CubeProgrammer v2.12.0 is available for download here.New Features (only some highlights):Script manager: add loops and conditional statements.STM32MP1: New SSP GUI.STM32 Trusted Packag...

Resolved! Using the STM32CubeProgrammer API

Hello!I am trying to use the STM32CubeProgrammer API to create my own application with a simple GUI in C++. Currently my solution is compiling the STM32CubePrgAPI as static library and then include it in a MFC project.Basically user clicks OK from th...

rtl by Associate II
  • 2601 Views
  • 1 replies
  • 0 kudos

Unable to connect (& hence flash the firmware) the STM32-Cube-Programmer with STM32-target-board in USB-DFU-mode if loaded firmware is read-protected.

1) I am able to connect the STM32-Cube-Programmer in USB-DFU-mode if existing or loaded firmware in to STM32-target-board is not read-protected.Image-1: Able to connect with target boardImage-2: Able to load firmware in to target board2) I am not abl...

0690X000009Z7piQAC.png 0690X000009Z7qWQAS.png 0690X000009Z7rUQAS.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.