2020-05-17 1:00 PM
I have an STM32F030K6T6, I 'm using STM32CubeProgrammer with ST-Link V2.
I click 'connect' and I get this error:
'Error: Data read failed'
It gets connected to the MCU, reads correctly it's ID.
I have checked all related connections: SWCLK, SWDIO, RST, 3V3 and GND. (I 'm not using the SWIM).
Everything looks ok.
I 've tried both options of BOOT0 (grounded & pulled up to 3V3).
So what might be the problem? A damaged MCU? (maybe I overheated it during soldering)
And if it 's damaged how does it get recognized by the STM32CubeProgrammer?
2020-09-30 11:07 AM
uncheck read protection byte
2021-10-18 8:19 AM
It helped to me (STM32CubeProgrammer >> OB >> Read Out Protection >> RDP = AA) when I had a similar issue with the STM32WB55CGUx. However, I did not set this byte myself. I just used the STM32CubeIDE to flash the memory. It happened once out of tens of program uploads.
2022-12-01 3:24 AM
Edit: it turned out to be a burned Chip, 12v low current was leaking back to my MCU so it was messingup with the pin cmos and nothjign else.
__________________________________________
I have a similar issue, somehow i corrupted the oB bytes when launching a debug session with cubeIDE. (nucleo- stm32f207ZG)
I am not able to read anything from the chip
Error: Data read failedi am able to read the OB no problem BUT, i cannot change the RDP from FF to AA
12:21:08:801 : OPTION BYTE PROGRAMMING VERIFICATION:
12:21:08:802 : Error: Expected value for Option Byte "RDP": 0xAA, found: 0xFF
12:21:08:821 : Error: Option Byte Programming failedHere they suggest something wrong with stlink the connectivity....( which is not my case because its a nucleo board)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.