2022-11-29 2:24 AM
Hello!
I am trying to use the STM32CubeProgrammer API to create my own application with a simple GUI in C++. Currently my solution is compiling the STM32CubePrgAPI as static library and then include it in a MFC project.
Basically user clicks OK from the GUI and then Example2 is executed. The getSTLinkList function executes with no issues, but connectSTLink fucktion gives me this error.
int connectStlinkFlag = connectStLink(debugParameters);
0xC0000005: Access violation executing location 0x0000000000000000.If I compile STM32CubePrgAPI as .exe, it works with no problems.
What am I not understanding? Is compiling it as a static library a valid choice? What other options do I have?
I can't find any examples of applications created using this API. Has anyone done something like this?
Solved! Go to Solution.
2022-11-29 3:31 AM
Initially I excluded the progress bar and message display functions callbacks, because I thought they weren't needed for my use case as I am not using the CLI. Apparently it is needed and adding it fixed my issue. Can anyone explain, why?
/**
* \brief This routine allows to choose your custom display.
* \param c : Fill the struct to customize the display tool.
* \note This function must be called first of all to ensure the display management.
*/
void setDisplayCallbacks(displayCallBacks c); displayCallBacks vsLogMsg;
/* Set the progress bar and message display functions callbacks */
vsLogMsg.logMessage = DisplayMessage;
vsLogMsg.initProgressBar = InitPBar;
vsLogMsg.loadBar = lBar;
setDisplayCallbacks(vsLogMsg);
2022-11-29 3:31 AM
Initially I excluded the progress bar and message display functions callbacks, because I thought they weren't needed for my use case as I am not using the CLI. Apparently it is needed and adding it fixed my issue. Can anyone explain, why?
/**
* \brief This routine allows to choose your custom display.
* \param c : Fill the struct to customize the display tool.
* \note This function must be called first of all to ensure the display management.
*/
void setDisplayCallbacks(displayCallBacks c); displayCallBacks vsLogMsg;
/* Set the progress bar and message display functions callbacks */
vsLogMsg.logMessage = DisplayMessage;
vsLogMsg.initProgressBar = InitPBar;
vsLogMsg.loadBar = lBar;
setDisplayCallbacks(vsLogMsg);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.