STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32F7 dual bank mode vs flashing tools

Don't have a eval board currently, waiting for order to arrive.Can anyone tell whether CubeProgrammer and other popular tools will properly detect that F7 is in dual bank mode, so it has a different number and size of sectors?Can these tools set the ...

Pavel A. by Super User
  • 2137 Views
  • 2 replies
  • 0 kudos

Hi all, MCU we are using is :- STM32G0B1CE During factory manufacturing we have notice some issues where MCU does not enumerate the comport.

We have seen several signatures of this issue.Signature 1:The extracted binary shows that the image is located on Bank1. Also the extracted byte options show that the image should be located on Bank2 but it was empty and still the device boots up aft...

Kpodu.1 by Associate II
  • 2236 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeProgrammer (cli) chunk size setable?

Heyin a project of us we are using the legacy STMFlashLoader to flash firmware on a STM32F103 via the system bootloader on UART1, but wanted to migrate to STM32CubeProgrammer now. In this application the PC (Win10) which runs STMFlashLoader/STM32Cube...

waldmanns by Associate II
  • 1808 Views
  • 1 replies
  • 1 kudos

Resolved! STM32CubeProgrammer USB DFU not detected on linux

Hi,USB DFU did not work in STM32CubeProgrammer in Linux. The programm did not detect the usb port. But it works faultless in STM32CubeProgrammer in windows.I tested with STM32CubeProgrammer V2.10 and 2.12, same results.I have linux mint 20.3 Luna

0693W00000WL7ZIQA1.png
VNong by Associate II
  • 12111 Views
  • 4 replies
  • 1 kudos

Flow control issues with CP2102

When using STM32CubeProgrammer and Silicon Labs CP2102 for USB-UART bridge, DTR state does not become "1 (Low)" when read unprotecting. No problem with FTDI FT232RQ.Our system uses DTR for RXD control, so if DTR is 0 (High), communication is not poss...

MYabe.1 by Associate
  • 1571 Views
  • 0 replies
  • 0 kudos

Resolved! Programming STM32H750B-DK discovery board failed

Trying the program STM32H750B-DK discovery board using STM32CubeProgrammer, but it fails. Here is the log: 08:47:43 : STM32CubeProgrammer API v2.11.0 | Linux-64Bits  08:47:45 : ST-LINK SN : 0036004A3137511133333639 08:47:45 : ST-LINK FW : V3J10M3 08:...

Ehsan by Associate II
  • 2583 Views
  • 6 replies
  • 0 kudos

Resolved! UART DFU on stm32l475

Hi,I am attempting to jump to system memory to be able to update the firmware via UART. Due to design constraints, BOOT0 pin will not an option for accessing the bootloader thus jumping to system memory within the application is needed.I'm using the ...

TJime.1 by Associate
  • 1655 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.