2017-02-23 12:43 PM
I am using atmega AT24C256 EEPROM and STM32F0 discovery module. I am struggling to read/Write to the memory. Here is the example I trying to use:-
&sharpdefine I2C1_DEVICE_ADDRESS 0x50 /* A0 = A1 = A2 = 0 */
&sharpdefine MEMORY_ADDRESS 0x07Buffer[0] = 'M';
HAL_I2C_Mem_Write(&hi2c1, (uint16_t) I2C1_DEVICE_ADDRESS<<1, MEMORY_ADDRESS, 1, Buffer, 1, 5); HAL_Delay(1000); Buffer[0] = 0x00; HAL_Delay(1000); HAL_I2C_Mem_Read(&hi2c1, (uint16_t) I2C1_DEVICE_ADDRESS<<1, MEMORY_ADDRESS, 1, Buffer, 1, 5); if (Buffer[0] == 0x4D) // if xBuffer[0] = 'M' { Test = 1; }On reading from memory, I do not get the 'M' or but some '255' instead. Where is the problem? Do I need to configure clock properly? I used CUBEMX for basic routines.
#cubemx #eeprom #hal #stm32f0 #i2c2017-03-07 8:34 AM
fixed it, just changed the mcu, mcu was sending i2c with some strange spikes i saw on my portable oscilloscope, i guess thats why it did not work,
i used ur code and added
<<1 to the slave address, thanks.
Buffer[0] = 'M';
HAL_I2C_Mem_Write(&hi2c1, 0x57<<1, 0x0007, 2, Buffer, 1, 5);
HAL_Delay(10);
Buffer[0] = 0x00;
HAL_I2C_Mem_Write(&hi2c1,
0x
57<<1
,0x0007
, 2, Buffer, 0, 5);
HAL_I2C_Mem_Read(&hi2c1,
0x
57<<1
, 0x0007, 2, Buffer, 1, 5);2017-06-15 3:43 AM
I also have problem writing and reading the data EEPROM
My EEPROM DevAddress is 0xA0
the MSB bit of
DevAddress is 0 for writing and 1 for readeing.
val = HAL_I2C_GetState (&hi2c1);
print('HAL_I2C_GetState = %x', val);val = HAL_I2C_Master_Transmit (&hi2c1, (uint16_t) 0xA0, '
EEPROM
', 10, 10000);val = HAL_I2C_Master_Receive (&hi2c1, (uint16_t) 0xA1,&temp, 10, 10000);
am getting:
HAL_I2C_GetState = 20 //
0x20 i.e
HAL_I2C_STATE_READY = 0x20U, /*!< Peripheral Initialized and ready for use */
HAL_I2C_Master_Transmit error = 0HAL_I2C_Master_Receive error = 0HAL_I2C_Master_Receive data = ÿÿÿÿÿÿÿÿÿÿthnaks.
2017-06-15 7:44 AM
,
,
here is my ds3231 code, taken liberally from adafruit's library.
uint16_t ds3231_read_reg(uint16_t register_pointer)
,
{,
, , , HAL_StatusTypeDef status = HAL_OK,,
, , , uint8_t timeArray[7] = {0},, , ,while (HAL_I2C_IsDeviceReady(&,hi2c1, (uint16_t)(DS3231_ADDRESS<,<,1), 3, 100) != HAL_OK) {}
,
, , , status = HAL_I2C_Mem_Read(&,hi2c1, , , , , , , , , , , , , , , , , , , , , ,// i2c handle,
, , , , , , , , , , , , , , , , , , , , , (uint16_t)(DS3231_ADDRESS<,<,1), , , ,// i2c address, left aligned,
, , , , , , , , , , , , , , , , , , , , , (uint16_t)register_pointer, , , , , , ,// register address,
, , , , , , , , , , , , , , , , , , , , , I2C_MEMADD_SIZE_8BIT, , , , , , , , , , , , ,// ds3231 uses 8-bit register addresses,
, , , , , , , , , , , , , , , , , , , , , (uint8_t*)(&,timeArray), , , , , , , , , ,// place to put returned value,
, , , , , , , , , , , , , , , , , , , , , 7, , , , , , , , , , , , , , , , , , , , , , , , , , , ,// return seven bytes,
, , , , , , , , , , , , , , , , , , , , , 100), , , , , , , , , , , , , , , , , , , , , , , , ,// timeout, , , /* Check the communication status */
,
, , , if(status != HAL_OK),
, , , {, , , }
, , ,uint8_t ampm = 0,
,
, , ,uint8_t ss = , bcd2bin(timeArray[0] &, 0x7F),,
, , ,uint8_t mm = , bcd2bin(timeArray[1]),,
, , ,uint8_t hh = , bcd2bin(timeArray[2]),,
, , ,uint8_t d , = , bcd2bin(timeArray[4]),,
, , ,uint8_t m , = , bcd2bin(timeArray[5]),,
, , ,uint16_t y , = bcd2bin(timeArray[6]) + 2000,,
, , ,uint8_t dow = ((uint16_t)date2days(y,m,d) + 6) % 7,, , ,printf('%s, %s %d, %d , , ', dayNames[dow], monthNames[m], d, y),
, , ,if (hh == 12) {
,
, , , , , ,ampm = 1, // its 12:00pm,
, , , , , ,},
, , ,if (hh >, 12) {,
, , , , , ,hh -= 12, // 12hr mode - 13:00 is 1:00pm,
, , , , , ,ampm = 1,,
, , , , , ,},
, , ,if (hh == 0) {,
, , , , , ,hh = 12, // midnight is 12:00 am,
, , , , , ,ampm = 0,,
, , , , , ,}, , ,if (hh <, 10) {
,
, , , , , ,printf(' %d', hh),,
, , ,} else {,
, , , , , ,printf('%d', hh),,
, , ,},
, , ,printf(':%02d:%02d %s', mm,ss, amPmString[ampm]),, , ,printf('\r\n'),
, , , return bcdToDec(timeArray[0]),
,
}and here is my i2c initialization code, just as the STM32CubeMX application generated, for an L476 nucleo board.
/* Includes ------------------------------------------------------------------*/
,
♯ include 'i2c.h'♯ include 'gpio.h'
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
I2C_HandleTypeDef hi2c1,
/* I2C1 init function */
,
void MX_I2C1_Init(void),
{, hi2c1.Instance = I2C1,
,
, hi2c1.Init.Timing = 0x10909CEC,,
, hi2c1.Init.OwnAddress1 = 0,,
, hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT,,
, hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE,,
, hi2c1.Init.OwnAddress2 = 0,,
, hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK,,
, hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE,,
, hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE,,
, if (HAL_I2C_Init(&,hi2c1) != HAL_OK),
, {,
, , , Error_Handler(),,
, }, , , /**Configure Analogue filter
,
, , , */,
, if (HAL_I2CEx_ConfigAnalogFilter(&,hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK),
, {,
, , , Error_Handler(),,
, }}
void HAL_I2C_MspInit(I2C_HandleTypeDef* i2cHandle)
,
{, GPIO_InitTypeDef GPIO_InitStruct,
,
, if(i2cHandle->,Instance==I2C1),
, {,
, /* USER CODE BEGIN I2C1_MspInit 0 */, /* USER CODE END I2C1_MspInit 0 */
,
,,
, , , /**I2C1 GPIO Configuration , , ,,
, , , PB8 , , , , ------>, I2C1_SCL,
, , , PB9 , , , , ------>, I2C1_SDA,
, , , */,
, , , GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9,,
, , , GPIO_InitStruct.Mode = GPIO_MODE_AF_OD,,
, , , GPIO_InitStruct.Pull = GPIO_PULLUP,,
, , , GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH,,
, , , GPIO_InitStruct.Alternate = GPIO_AF4_I2C1,,
, , , HAL_GPIO_Init(GPIOB, &,GPIO_InitStruct),, , , /* Peripheral clock enable */
,
, , , __HAL_RCC_I2C1_CLK_ENABLE(),, , , /* Peripheral interrupt init */
,
, , , HAL_NVIC_SetPriority(I2C1_EV_IRQn, 0, 0),,
, , , HAL_NVIC_EnableIRQ(I2C1_EV_IRQn),,
, , , HAL_NVIC_SetPriority(I2C1_ER_IRQn, 0, 0),,
, , , HAL_NVIC_EnableIRQ(I2C1_ER_IRQn),,
, /* USER CODE BEGIN I2C1_MspInit 1 */, /* USER CODE END I2C1_MspInit 1 */
,
, },
}void HAL_I2C_MspDeInit(I2C_HandleTypeDef* i2cHandle)
,
{, if(i2cHandle->,Instance==I2C1)
,
, {,
, /* USER CODE BEGIN I2C1_MspDeInit 0 */, /* USER CODE END I2C1_MspDeInit 0 */
,
, , , /* Peripheral clock disable */,
, , , __HAL_RCC_I2C1_CLK_DISABLE(),,
,,
, , , /**I2C1 GPIO Configuration , , ,,
, , , PB8 , , , , ------>, I2C1_SCL,
, , , PB9 , , , , ------>, I2C1_SDA,
, , , */,
, , , HAL_GPIO_DeInit(GPIOB, GPIO_PIN_8|GPIO_PIN_9),, , , /* Peripheral interrupt Deinit*/
,
, , , HAL_NVIC_DisableIRQ(I2C1_EV_IRQn),, , , HAL_NVIC_DisableIRQ(I2C1_ER_IRQn),
, }
,
, /* USER CODE BEGIN I2C1_MspDeInit 1 */, /* USER CODE END I2C1_MspDeInit 1 */
,
}/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/**
,
, * @},
, *//**
,
, * @},
, *//************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
2018-01-21 10:30 PM
Hello, Am using STM32F0 uC for interfacing with a AT24C64. I am not able to write sequentially to the EEPROM after one page, i.e 32 Bytes. Can someone please if the logic is wrong.
This is the code:
data[0]=0x00; //First word address 8bit
data[1]=0x00; //Second word address 8bitfor(i=2;i<34;i++){data[i]=0x11;}HAL_I2C_Master_Transmit(&hi2c1, EEPROM_ADDRESS<<1, data, 34, 50); //data is int type,34 is number bytes of datadata[0]=0x00; //First word address 8bitdata[1]=0x20; //Second word address 8bit// Next Pagefor(i=2;i<34;i++){data[i]=0x22;}HAL_I2C_Master_Transmit(&hi2c1, EEPROM_ADDRESS<<1, data, 34, 50); //data is int type,34 is number bytes of datawhile (1){/* USER CODE END WHILE */data[0]=0x00;data[1]=0x00;HAL_I2C_Master_Transmit(&hi2c1, EEPROM_ADDRESS<<1, data, 2, 50); //data is int type pointing to first address herefor(i=0;i<32;i++){HAL_I2C_Master_Receive(&hi2c1, EEPROM_ADDRESS<<1, &dataout[i], 1, 50);//maximum is 32 byte data locations}data[0]=0x00;
data[1]=0x20;HAL_I2C_Master_Transmit(&hi2c1, EEPROM_ADDRESS<<1, data, 2, 50); //data is int type pointing to first address herefor(i=0;i<32;i++){HAL_I2C_Master_Receive(&hi2c1, EEPROM_ADDRESS<<1, &dataout_1[i], 1, 50);//maximum is 32 byte data locations}}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.