STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

User labels for peripherals

Posted on September 12, 2017 at 15:37I have had hands on the CubeMX user label feature for pin assignments and found it very usefull. It was possible to write application code like HAL_GPIO_TogglePin(my_label_GPIO_Port, my_label_GPIO_PIN), and when ...

STM32CubeMx size of generated code problem

Posted on December 21, 2017 at 14:44I am wroking on a project  using two microcontrollers a STM32F412 and a STM32L011 (8K flash, 2k RAM) .The STM32L011 is used as RTC to manage the power comsumption of the STM32F412. I used STM32CubeMx to generate t...

Unable to Read and Write to I2C EEPROM

Posted on February 23, 2017 at 21:43I am using atmega AT24C256 EEPROM and STM32F0 discovery module. I am struggling to read/Write to the memory. Here is the example I trying to use:-&sharpdefine I2C1_DEVICE_ADDRESS   0x50           /* A0 = A1 = A2 =...

anuj by Associate II
  • 10248 Views
  • 13 replies
  • 0 kudos

CubeMX on MacOS using far too much RAM

Posted on May 29, 2017 at 22:20CubeMX V4.21.0 on MacOS 10.12.5.4.21.0 was available, so I downloaded it. Opened my current project, checked to see if my pet peeves had been fixed yet - nope. Went for lunch.Came back from lunch and Cube has 3.7GB of ...

BUG in STM32CubeMX STM32L4 OPAMP ADC PROBLEM

Posted on June 08, 2016 at 16:48Hi, setting the ADC1_IN8 or ADC_IN15 as OPAMP x Output Differential  or OPAMP x Output Single-ended in STM32CubeMx v 4.15 with NUCLEO-L476RG doesn't generate the correct GPIO setup. The OPAMP output pins are configur...

Resolved! Trigger input capture every 8 rising edges

Posted on January 16, 2018 at 16:42Hey everyone,I'm using the stm32f722ze and CubeMx and have gotten my input capture working. Essentially, when every rising edge is detected, the timer triggers a DMA event and stores the GPIO pins value to memory. ...

con3 by Senior
  • 1520 Views
  • 3 replies
  • 0 kudos

CUBE Bug? hall sensor TRGO MasterSlave selection

Posted on January 18, 2018 at 05:36I am trying to configure the timers for a BLDC applications, so that the hall sensor change triggers another timer.In cube, If you configure a timer as XOR ON/ Hall Sensor Mode, you can't configure it as a Master T...

0690X00000609ECQAY.png
usama2 by Associate II
  • 915 Views
  • 0 replies
  • 0 kudos

Resolved! CubeMX problem (bug?)

Posted on March 08, 2017 at 14:33Hi,I'm having problems with STM32 CubeMX (v4.19.0) during the setup of the ADC2 peripheral (may be a bug...).Even if the number of conversion is ONE, I have two different ranks both pointing to the same ADC channel (...

flavio23 by Associate III
  • 4697 Views
  • 7 replies
  • 0 kudos

Cannot change USART1 interrupt priority in CubeMX

Posted on March 13, 2017 at 07:27In CubeMX 4.19.0 I have USART1 Asynchronous and FREERTOS enabled. USART1 global interrupt is enabled. In NVIC configuration dialog I have:USART1 global interrupt: On, Preemption priority 5, Sub priority 0, Uses FREER...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.