2025-10-06 8:12 AM
This is for an STM32F303.
I've reduced my MX configuration down as much as possible so that it only has SWD and a button on GPIO PA8 configured and the incorrect behaviour still occurs. The intent is for PA8 EXTI falling edge to start a timer, and for that timer to in turn interrupt on expiry. I do get an interrupt (for both EXTI and the timer), but the duration of the timer is always wrong (sometimes instant, sometimes quite slow), and when on interrupt I check instance->CNT it is always a random value.
Following https://community.st.com/t5/stm32cubeide-mcus/hal-tim-periodelapsedcallback-firing-very-prematurely/m-p/588486 I am issuing
hbuttonDebounceTimer->Instance->SR &= ~TIM_SR_UIF;during USER CODE 2 (after init, before the main loop), and it has no effect.
My ISRs look like
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) {
if (htim == buttonDebounceTimer) {
HAL_TIM_Base_Stop_IT(htim);
}
}
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
switch (GPIO_Pin) {
case nBUTTON_Pin:
HAL_TIM_Base_Start_IT(buttonDebounceTimer);
return;
}
}
Solved! Go to Solution.
2025-10-07 11:19 AM
Okay, so you think 55536 is a negative value. You keep doing you, I won't try to convince you otherwise anymore.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.