STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! TIM16 incorrect, random period

This is for an STM32F303.I've reduced my MX configuration down as much as possible so that it only has SWD and a button on GPIO PA8 configured and the incorrect behaviour still occurs. The intent is for PA8 EXTI falling edge to start a timer, and for...

avidroneg_0-1759763131044.png avidroneg_1-1759763166203.png
avidroneg by Associate III
  • 1460 Views
  • 10 replies
  • 1 kudos

Resolved! Can't configure USB Host for STM32WBA on STM32CubeMX

I'm trying to use STM32CubeMX directly or via STM32CubeIDE, and I can't find a way to configure ThreadX + USBX Host for STM32WBA65 boards such as NUCLEO-WBA65RI or STM32WBA65I-DK1.    Only Device classes show up.I've also tried to do it using the par...

noela by Associate II
  • 905 Views
  • 4 replies
  • 0 kudos

Resolved! IDE and STM32H723: Issue with DMAs and ADC handlers name

This (DMA_STR0_IRQHandler) won't, but this (DMA1_Stream0_IRQHandler) is work-fine.Clearly, the naming and cases are different, but these two handlers are part of startup file, were generated from two different projects options (Empty and Cube MX) for...

APatr.1 by Associate II
  • 674 Views
  • 2 replies
  • 3 kudos

Resolved! Error with CMake in New Version 6.15.0

Today, while using the CubeMX product, I upgraded to version 6.15.0 (previously 6.14.1). After upgrade, the CMake step when generating project code failed. Even when generating an empty project, CMake still did not succeed. I also tried previously wo...

Mocozzz by Associate II
  • 5061 Views
  • 13 replies
  • 5 kudos

Resolved! CUBEMX 6.15 with Keil Full Assert bug

Same problem here (Cube 6.15.0, Keil uVision  Although HAL is selected, Cube installed both HAL and LL files for ADC and some other peripherals by mistake.  which results in a compile error ../Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_ll_adc.c(25...

regjoe_2-1758639075547.png regjoe_0-1758638667389.png regjoe_1-1758639027356.png
regjoe by Senior II
  • 1148 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.