2026-03-18 9:56 PM
Hello, I am using the STM32H503 MCU. When I configure the pins as follows:
PB2 → OUTPUT
PA8 → TIM1_CH1
PB7 → I2C1_SDA
In the RCC section, I get red warnings for Master Clock Output1 (MCO), LSCO clock output, and SAI1 External clock. I cannot disable these clock settings. Is there a way to do this in CubeMX? How can I resolve this conflict in CubeMX?
2026-03-18 10:37 PM
What conflict?
These are just warnings signaling that you cannot use some function cause you activated another function on some pins.
2026-03-19 12:27 AM
Hello @r2-d2 and welcome to the ST community,
Please share your ioc file so we can check.
2026-03-19 5:58 AM - edited 2026-03-19 5:59 AM
What do the warnings say? Hover over them for context. Probably they are informational and can be ignored.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.