STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

stm32f334 HRTIM STM32CubeMX bug

Hi. I want to use the A HRTIM timer to independently control two MOSFETs. Namely, I have a transformer with the midpoint connected to the positive pole of the power supply, and these two transistors switch the 2 halves of the winding as lower switche...

ATymo1_0-1765047172541.png
ATymo.1 by Associate II
  • 871 Views
  • 3 replies
  • 1 kudos

Resolved! Inconsistent pin naming

I've always found it a little irritating:#define CLK_A_Pin GPIO_PIN_0 #define CLK_A_GPIO_Port GPIOFWhy is it deemed necessary to have "GPIO" in one, but not the other? Surely, that should be either:#define CLK_A_GPIO_Pin GPIO_PIN_0 #define CLK...

stm32h503xx Clock ..

Hello, I am using the STM32H503 MCU. When I configure the pins as follows:PB2 → OUTPUTPA8 → TIM1_CH1PB7 → I2C1_SDAIn the RCC section, I get red warnings for Master Clock Output1 (MCO), LSCO clock output, and SAI1 External clock. I cannot disable thes...

r2-d2 by Associate
  • 391 Views
  • 3 replies
  • 4 kudos

Resolved! Adding Source Files to CMake Project

Hi all, I've been using CubeIDE for a little while and decided to build my next project using the STM32 VSCode extensions, which I am still figuring out. I am also figuring out CMake for the first time, as I let CubeIDE handle all the build details p...

ghincher by Associate
  • 1076 Views
  • 2 replies
  • 2 kudos

How to Set Up the Full CUBEMX on the STM32N6570-DK Board

안녕하세요 STM32N6570-DK의 사용하기 위한 cubemx 설정이 필요합니다. 카메라, lcd, sd카드, usb, eth 등 기능을 다 살린 cubemx 설정 또는 ioc 파일을 받고 싶습니다. 확인 부탁 드립니다.   Hello, I need a cubemx setting for use of STM32N6570-DK. I would like to receive a cubemx setting or an ioc file that utili...

LeeJaewon by Associate III
  • 453 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.