2020-08-05 11:55 AM
Hello, i have got problem with basic project form STM32CubeMX. Help please.
This is my project https://drive.google.com/file/d/1nJh5805ZFjzibTgeT_i-kSdNzgrmXk0_/view?usp=sharing for STM32CubeMX
I write in SW4STM32 main.c:
* USER CODE BEGIN Includes */
#include "lwip/opt.h"
#include "lwip/arch.h"
#include "lwip/api.h"
#include "usbd_cdc_if.h"
/* USER CODE END Includes */
And I compile the project with "Optimization level -O0" and "Debug level None".
I do .dfu file with DfuFileMgr.exe and load program with DfuSeDemo.exe. Successful.
Driver Virtual Com Port for STM32 version 2.1.0.
Problem: Putty don't open Virtual Com Port. Why is this happening?
If you reduce the number of threads the port opens. But this option is not suitable.
Solved! Go to Solution.
2020-08-06 5:08 PM
The more flawed code you stick together, the less are the chances of something working at all. In case of RTOS + lwIP + USB slapped together by CubeMX the chances are approaching zero.
2020-08-05 8:12 PM
Does your program hard fault as a result of more threads? When you debug it, are things still executing? Possible you just ran out of stack/heap room.
2020-08-06 12:04 PM
No, the program does not have hard fault. An empty project generated by STM32CubeMX has a heap/stack overflow?
2020-08-06 12:31 PM
Doesn't look like an empty project to me. But yes, even a trivial program can overflow the stack/heap if those are set too small.
2020-08-06 5:08 PM
The more flawed code you stick together, the less are the chances of something working at all. In case of RTOS + lwIP + USB slapped together by CubeMX the chances are approaching zero.
2020-08-07 10:02 AM
What are the options? Other libraries and IDEs?
2020-08-08 7:41 AM
Do you know how to detect stack/heap overflow? I haven't found any information on this topic yet...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.