2020-07-27 2:46 AM
What is new in STM32CubeMX V6.0.0?
Added the support of new part numbers in the STM32G4 Series: STM32G491K(C-E)Ux, STM32G491C(C-E)Ux, STM32G491C(C-E)Tx, STM32G491REYx, STM32G491R(C-E)Tx, STM32G491R(C-E)Ix, STM32G491M(C-E)Sx, STM32G491M(C-E)Tx, STM32G491V(C-E)Tx, STM32G4A1KEUx, STM32G4A1CEUx, STM32G4A1CETx, STM32G4A1REYx, STM32G4A1RETx, STM32G4A1REIx, STM32G4A1MESx, STM32G4A1METx, and STM32G4A1VETx
Added the support of new part numbers in the STM32H7 Series: STM32H723x, STM32H725x, STM32H730x, STM32H733x and STM32H735x
Added the support of one new part number in the STM32F4 Series: STM32F479IIHx
Added the support of three new part numbers in the STM32F7 Series: STM32F723V(C-E)Tx and STM32F733VETx
Added the support of new part numbers in the STM32L0 Series: STM32L031C4Ux, STM32L041C6Ux, STM32L051C(6-8)Ux, STM32L052C(6-8)Ux, STM32L053C(6-8)Ux, STM32L062C8Ux, STM32L063C8Ux, STM32L071C8Ux, STM32L082KBUx and STM32L083RBTx
Added the support of new part numbers in the STM32L1 Series: STM32L162QCHx, STM32L162VDYxX and STM32L162ZCTx Added the support of new part numbers in the STM32L4 Series: STM32L496VGTxP, STM32L496VGYxP and STM32L4A6VGTxP
Added the support of one new part number in the STM32WB Series: STM32WB55VYYx
Added the support of new boards: NUCLEO-G491RE, STM32H735G-DK, NUCLEO-H723ZG, NUCLEO-WB55RG, B-L462E-CELL1, B-L4S5I-IOT01 and STM32MP157F-EV1
Added the video tutorials feature to access video tutorials on various STM32CubeMX features
Added the support of an Example Selector that enables example filtering among several parameters
Added the support of PCC for the STM32L5xQ part numbers with SMPS
Software Packs: – User interface enhancements with simplified access to Software Pack installation and component selection from the Pinout&Configuration view and to Software Pack documentation from the Component Selector window – Implementation aligned with Arm® CMSIS-Pack 1.6.3 revision
Added a graphical tool, named STM32PackCreator and installed with STM32CubeMX in the Utilities folder. It allows pack developers to create Software Packs and STM32Cube Expansion packages enhanced for STM32CubeMX. It can be launched from the ST Tools tab found in the STM32CubeMX Tools view.
STM32CubeIDE toolchain:
It is functional only with a Java 8 64-bit Java Virtual Machine.
Example Selector:
The feature is functional only for the examples related to the STM32F4, STM32F7, STM32G0, STM32G4, STM32H7, STM32L5 and STM32WB Series
Software Packs:
When a pack is disabled, generated files are not removed from the project
– Workaround: remove these files manually
Possible issue with component dependencies in the Additional Software components selection window
– Workaround: click on the Refresh button from the Embedded Software Packages Manager
When using the GNSS pack, users must not migrate their project from 3.x to 4.0.0
Functionalities not supported:
– maxInstances, isDefaultVariant, generator attributes of the component element
– Dtz, Ddsp, Dsecure attributes of the condition element
– repository element – tag and url attributes of a release element
– dominate element
– public attributes for the file element
– preIncludeLocal and preIncludeGlobal file category attributes
– Pre_Include_Local_h element
– Pre_Include_Global_h element
– Pack components where attribute values come with a "." character
Link
https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-configurators-and-code-generators/stm32cubemx.html
2020-08-08 9:13 AM
Installed the very first time a STM-Software. CubeMX only shows the Startscreen, then nothing. No Program, no entry in Windows-Taskmanager, nothing
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.