2021-04-21 6:25 AM
Rationale:
I have several projects on the same MCU that evolve almost simultaneously. (However, the pinout is different). When adding new features, I have to enable some of them in GUI mode several times. `sort`ing the contents of *.ioc files alphabetically and `diff`/merging helps in part.
Is it possible to fully automate the creation of a * .ioc file from a script (STM32CubeMX -q script.txt)?
script.txt:
swmgr install stm32cube_h7_1.9.0 accept
load STM32H743VITx
project name M7_MODBUS
project toolchain SW4STM32
SetStructure Advanced
SetCopyLibrary "copy only"
project couplefilesbyip 1
# Working, ip "CORTEX_M7" available
set ip parameters CORTEX_M7 CPU_ICache Enabled
set ip parameters CORTEX_M7 CPU_DCache Enabled
# Not working. How to click "Activated" checkbox (enable) on IWDG1 via this script?
set ip parameters IWDG1 Reload 4000
set ip parameters IWDG1 Window 4000
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.