2016-09-01 4:22 AM
Hi, I am using a nucleo - F103RB board for testing its UART. I am using the STM32Cube Mx to generate the codes for the start. I can successfully generate working codes for Usart1 and it can successfully transmit and receive using the HAL library. But when I generate codes for Usart2 using the STM32Cube, I can no longer transmit or receive any data. Does the STM32cube not generate all the required codes for USART2? I am quite new to this so please explain why USART1 is different than USART2 in this case.
here is the auto generated code for the USART2 void MX_USART2_UART_Init(void) { huart2.Instance = USART2; huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart2) != HAL_OK) { Error_Handler(); } } void HAL_UART_MspInit(UART_HandleTypeDef* uartHandle) { GPIO_InitTypeDef GPIO_InitStruct; if(uartHandle->Instance==USART2) { /* USER CODE BEGIN USART2_MspInit 0 */ /* USER CODE END USART2_MspInit 0 */ /* Peripheral clock enable */ __HAL_RCC_USART2_CLK_ENABLE(); /**USART2 GPIO Configuration PA2 ------> USART2_TX PA3 ------> USART2_RX */ GPIO_InitStruct.Pin = GPIO_PIN_2; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_3; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* Peripheral DMA init*/ hdma_usart2_rx.Instance = DMA1_Channel6; hdma_usart2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_usart2_rx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_usart2_rx.Init.MemInc = DMA_MINC_ENABLE; hdma_usart2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE; hdma_usart2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE; hdma_usart2_rx.Init.Mode = DMA_CIRCULAR; hdma_usart2_rx.Init.Priority = DMA_PRIORITY_LOW; if (HAL_DMA_Init(&hdma_usart2_rx) != HAL_OK) { Error_Handler(); } __HAL_LINKDMA(uartHandle,hdmarx,hdma_usart2_rx); /* Peripheral interrupt init */ HAL_NVIC_SetPriority(USART2_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USART2_IRQn); /* USER CODE BEGIN USART2_MspInit 1 */ /* USER CODE END USART2_MspInit 1 */ } } #usart2 #stm32f102016-09-05 1:12 AM
I flagged this query to Tech support and they told me about
USART communication
The
USART2
interface available on PA2 and PA3 of the STM32 microcontroller can beconnected to ST-LINK MCU, ST morpho connector or to Arduino connector. The choice can
be changed by setting the related solder bridges. By default the USART2 communication
between the target MCU and ST-LINK MCU is enabled, in order to support Virtual Com Port
for mbed (SB13 and SB14 ON, SB62 and SB63 OFF). If the communication between the
target MCU PA2 (D1) or PA3 (D0) and shield or extension board is required, SB62 and
SB63 should be ON, SB13 and SB14 should be OFF. In such case it is possible to connect
another USART to ST-LINK MCU using flying wires between ST morpho connector and
CN3. For instance on NUCLEO-F103RB it is possible to use USART3 available on PC10
(TX) and PC11 (RX). Two flying wires
need to be connected as follow:
•PC10 (USART3_TX) available on CN7 pin 1 to CN3 pin RX
•PC11 (USART3_RX) available on CN7 pin 2 to CN3 pin TX
So I disconnected the
SB13
andSB14
soldering points to disable the USART2 for debugging, connectedSB62
andSB63
soldering points to enable pins at PA2(TX) and PA3(RX) and then connected PC10 to CN3 pin RX, PC11 to CN3 pin TX to enable USART3 for debugging.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.