2022-04-26 3:00 PM
A very strange things happened when trying to browse (open a project) on most of the directories located on my MAC (OS Monterey on Apple M1 MAX):
The directories informations looks identical (see the pictures)
Can you please explain what is the reason? I use the latest STM32CubeMX.
Thanks,
Andrei
Solved! Go to Solution.
2023-03-29 12:54 PM
What worked for me is to add STM32 Cube MX to list of the apps that get allowed "full disk access" under System Preferences -> Privicay & Security -> Full Disk Access.
2023-01-24 10:14 PM
Hi @Community member , have you been able to solve this issue? I'm facing the same issue.
2023-02-14 6:29 AM
Any updates here. I have the same issue and believe it could be connected to security features of OS X and bad programming from ST side... The tool almost unusable since I can not load old files. On one installation of OS X (Monterey) I can't even store the file-settings.
2023-03-29 12:54 PM
What worked for me is to add STM32 Cube MX to list of the apps that get allowed "full disk access" under System Preferences -> Privicay & Security -> Full Disk Access.
2023-03-29 1:46 PM
Ye this solve the problem. I'm not sure how safe it is as CubMX can erase with no asking an entire directory...
But works!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.