STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Don't see DAC output for SINE wave with DMA

Hello,I followed a tutorial on how to generate a SINE wave using DAC and DMA that was really good. Logically it makes sense, you set up the DAC, set it to be triggered by a timer, then set up the DMA channel, set it to circular, and set it to use a t...

0693W00000FAgEAQA1.png 0693W00000FAgE5QAL.png 0693W00000FAgEFQA1.png 0693W00000FAgEeQAL.png

Resolved! Why is the clock config error?

Hi, when I use the cubemx to config the stm32h743iit6 project, the clock system shows some error as below. But I try it on another PC, and the same config can work well.I don't know why?

0693W00000aJZg9QAG.png
Junde by Senior III
  • 1665 Views
  • 3 replies
  • 0 kudos

Resolved! How to properly open projects with the extention?

Hello,I followed all instructions and created new example project in CubeMX for CubeIDE. Then I used the vsCode extention to import an existing project with the .cproject file. How should you now open the linked source files to be able to edit the fi...

0693W00000aJKdUQAW.png
MFran.14 by Associate
  • 2733 Views
  • 2 replies
  • 0 kudos

Why Pullup on LEDs ?

When using STM32CubeIDE 1.12.0 with a NUCLEO-U575ZI-Q, the code generated use pullup for the LEDs. It become impossible to achieve low power with those pullup.

nicolas by Senior II
  • 2592 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.