2023-03-09 6:38 AM
I have installed Xcode and tried to run the instructions "In case of error, try one of the following fixes: - $sudo xattr -cr ~/SetupSTM32CubeMX-6.8.0.app."
2023-03-29 4:16 AM
Hello @CColo.2
First let me thank you for posting .
Let's try to uninstall and reinstall CubeMX again .
This is the LINK to download the Latest version CubeMX 6.8.0
Uninstalling STM32CubeMX on macOS® :
There are two different ways to uninstall STM32CubeMX on Mac:
1. Move STM32CubeMX.VERSION.app to the trash
2. Use the following command line:
a) For STM32CubeMX 6.2.x and later versions only: cd SetupSTM32CubeMX-VERSION.app/Contents/Resources/Uninstaller ./uninstall.s
To install CubeMX 6.8.0 On macOS please follow those steps :
a) On STM32CubeMX-Mac line, Click “Get software�? to download the package
b) Extract (unzip) the downloaded package.
c) Make sure you have administrator rights.
d) Double-click SetupSTM32CubeMX-VERSION.app application file to launch the
installation wizard.
In case of error, try to fix it: - $sudo xattr -cr <Folder where the zip was extracted>
Thx
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-29 8:02 AM
Hello Ghofrane GSOURI,
Thank you, the problem I had was the Beta version of macOs Ventura 13.3, it wouldn't let me install the software, I reinstalled the normal Ventura 13.3 version, I installed the CubeMX 6.8.0 version without a problem and then I updated to the Beta version of the macOS.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.