2024-05-22 1:57 AM - last edited on 2024-06-04 7:08 AM by Peter BENSCH
Hi All!
Using STM32CubeMx 6.11.1, and the STM 32L475 processor, I have successfully configured UART 5 to use DMA with interrupts on TX and just interrupts (no DMA) on receive. But whatever I do, STM32Cube seems to generate these lines:
/* UART5 interrupt Init */
HAL_NVIC_SetPriority(UART5_IRQn, 10, 0);
HAL_NVIC_EnableIRQ(UART5_IRQn);
which I don't want - enabling the interrupts before certain initialization is not what I want. On the NVIC category, and tab 'Code generation' I have unchecked the 'Generate Enable in Init':
I have tried removing the use of DMA but still get this interrupt initiailization.
Any ideas on what could be happening and how I can stop this interrupt initialization occuring?
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.