2026-04-23 9:59 AM
Hello,
For one of my project, my goal is to use PTP to synchronise multiple STM32H563 to one host.
However, when configuring the ETH Device, I can only enable RMII, as the "RMII_PTP_SYNCHRO" is greyed out.
I've read the pop up that tells me to enable TIM2 as a slave with trigger source "ETR1 through Remap", Channel 1 as "Input Capture direct mode from Remap".
And both "remap capabilities" are set to "is connected to ETH_PPS".
Is there something that I'm missing ?
Best regards
2026-04-27 5:24 AM
Hello @AMouton
Thanks for highlighting this behavior,
I will check it internally and get back to you ASAP.
KR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-04-28 9:10 AM
Hello @Souhaib MAZHOUD !
If that can help you, I'm running CubeMX 6.17.0 (and I've tried with older versions too)
I've looked through the STM32H5 & STM32H7 examples and never found an example where RMII_PTP_SYNCHRO is enabled. I believe the check condition for where the option is available is problematic on all STM32Hx models.
Is there any way I can help you or your team to troubleshoot this ?
Regards,
Albin Mouton
2026-04-30 1:38 AM
Hello @AMouton
Thanks for your detailed explanation.
This issue has been escalated to dedicated team for further investigation: Internal ticket number: CDM0062262 (This is an internal tracking number and is not accessible or usable by customers.)
BR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-04-30 2:43 AM
2026-05-07 9:02 AM
Hello @ACR
The condition in N6 is not the same as in H5. To enable ETH in RMII_PTP_SYNCHRO mode with N6, you have to activate TIM2/TIM3 slave mode with ITR4 as trigger source or if FDCAN is enabled.
KR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.