STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Fixing code generation in CubeMX: Tickless functions

Hello, when using CubeMX + STM32WB + BLE, I noticed that if the BLE feature is enabled in CubeMX, a file called freertos_port.c is created in the project. This file includes the functions void vPortSuppressTicksAndSleep(TickType_t xExpectedIdleTime) ...

JJRR by Senior
  • 2689 Views
  • 4 replies
  • 0 kudos

STM32F4 CAN Bus example using HAL Library

Posted on April 22, 2016 at 18:51Hello,   i am new to HAL Libraries. i am learning to work with CAN BUS using HAL Libraries. Can any one please post an example of STM32F CAN BUS using HAL Libraries.as it will help to have an idea how should we progr...

ninad911 by Associate III
  • 36067 Views
  • 18 replies
  • 0 kudos

Resolved! IOC file lifetime in project development

Hi, how long do you recommend that we keep our development project's in-sync with the IOC file used to generate them? Setup:MyNewDemo.ioc is used to create a demo monitoring the UART that responds to to toggle requests for its GPIO Scenario #1:Periph...

jreina by Associate III
  • 2649 Views
  • 3 replies
  • 2 kudos

STM32F407 ETH Problem

Hi Everyone,I cannot choose the speed of the Eth. Pls see the pisture below. The version of the STM32CUBEMX that I downloaded is the latest.Best regards,Jason Pls see the picture.Best regards,Jason

STM32F407VET6 ETH.png
Xinda by Associate
  • 1059 Views
  • 1 replies
  • 0 kudos

How to add a lib to CMake project generated by STM32CubeMX

Hello,When generating a CMake project with STM32CubeMX, it generate a library stm32cubemx defined as an interface.I created a libPWM. To have all the compile/CPU/drivers hal informations, my libPWM must be linked to the stm32cubemx.To avoid error, in...

ANauz.1 by Senior II
  • 1455 Views
  • 0 replies
  • 0 kudos

STM32Cube: Generate code from command line with no GUI

Posted on June 14, 2018 at 17:59Hi!I have a project based on STM32. The project can be configured to run on several STM32 boards.Each board configuration is represented by the `.ioc` file created by CubeMX.I want to have a CI (Continuous Integration...

0690X0000060BfYQAU.png

LWIP_NUM_SYS_TIMEOUT_INTERNAL does not have LWIP_SNTP in it.

When I enabled SNTP I got an error message that basically said there were not enough timers. When I disabled it, the error went away. I had to add LWIP_SNTP to the define for LWIP_NUM_SYS_TIMEOUT_INTERNAL in opt.h. However, every time I Generate C...

MStra.3 by Associate III
  • 3455 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.