2017-10-19 10:13 PM
I have a brand-new STM32F303 Nucleo144 and cannot get any CubeMX generated apps to work with USB. The app builds and runs fine, and I can see printf output via SWO, but the device never evenbegins enumeration. The following procedure was used to develop a minimal reproducible example:
Plugging and unplugging the device's user USB port does nothing on the PC - not even showing an unknown device. Device Manager does not attempt a refresh (which is visually quite noticeable) when you plug in the device. So the failure is at a very early stage, perhaps not even beginning to enumerate. This leads me to suspect perhaps a clock or interrupt issue.
I have tried many fixes, including the following changes, and nothing helps at all:
I also tried starting from scratch and following along with the official STM tutorial as shown in this video:
But that didn't work either. Thinking perhaps there was some faulty hardware, I tried another board. Still nothing. I've tried nearly every suggestion I could find in the forums.
TheUSB HAL code that ships with theSDK is not actually generated by CubeMX (and doesn't have gcc Makefiles) so it's not really that useful.
So is there a minimalist USB example that is actually generated from CubeMX that actually works?
Thanks -
:: Gavin
https://community.st.com/tags#/?tags=stm32%20cubemx
https://community.st.com/tags#/?tags=usb
#stm32-cubemx #usb Note: this post was migrated and contained many threaded conversations, some content may be missing.Solved! Go to Solution.
2017-12-21 10:08 AM
As long as the USB peripheral of the device has the DPPU bit in the BCDR register, external pull-up resistor isn't necessary. The F0 line has this, so your problem is rooted somewhere else.
2018-01-09 7:24 AM
Ben,
I have taken USB CDC sample code from stm32cubef0 and modified for STM32F070RB and tried in NUCLEO-F070RB. Now i am seeing USB enumeration and it is coming under ports. When i flash same code on development board, USB enumeration is not happening. When we cross verified schematics with nucleo booard, we are not seeing any difference for USB section. is there any bootloader difference will be there from controller what we get from STM and nucleo board? or any other extra configuration needed in code specific to development board
2018-01-09 9:28 AM
Does the dev board have the same type of MCU on it as the Nucleo?
There is a quite simple way to check if the physical USB connection is correct: pull BOOT0 high so the device enters system memory boot mode. This mode provides a USB DFU interface which should be detected by the PC.
Generally these steps should be followed to detect trivial errors in USB setup:
1. The Reset interrupt is not generated by the USB upon connection (with D+ pullup active)
→ physical line problem
2. The Setup interrupt is not generated
→
USB clocking issue
3. The device doesn't enter configured state, stays in addressed
→
either device software or PC side driver issue (e.g. invalid descriptor)
2018-01-09 10:13 AM
Dev board is having same MCU as Nucleo board.
Do we need pullup for this controller?
Without enabling pullup, same code is working fine in Nucleo board.
Software level do we need to have any changes in code from nucleo board to dev board.
2018-01-10 2:23 AM
Do we need pullup for this controller?
I have answered this
https://community.st.com/0D50X00009XkXRtSAN
.Software level do we need to have any changes in code from nucleo board to dev board.
Since the pins are mapped identically, you only need to adjust your system clock settings.For USB you better be using HSE clock source (since HSI48 isn't available in F070), make sure the PLL output is 48 MHz.
2018-01-10 8:05 AM
Do we need external oscillator?
I have used below code to generate PLL as 48MHz.
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6;
RCC_OscInitStruct.PLL.PREDIV = RCC_PREDIV_DIV1;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USB;
PeriphClkInit.UsbClockSelection = RCC_USBCLKSOURCE_PLL;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
But the same code is working fine in F070 nucleo board. That is the reason i am not able to differentiate issue.
2023-09-24 1:19 AM
6 years later, CubeMX still does the same mistake for L1
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.