2018-11-23 1:45 PM
Hello
In glass LCD display configuration (for STM32L152RB in my case), for static display, in Cube we can see segment numbers SEG[0-31]. Meanwhile, SEG[31:28] are double numbered, also to SEG[43:40]. To use [31:28] designators there must be MUX_SEG bit in LCD_CR set.
After code generation MUX_SEG is still disabled (0). I found the line in MX_LCD_Init function:
hlcd.Init.MuxSegment = LCD_MUXSEGMENT_DISABLE;
And i can't find proper setting in Cube to enable this MUX, i has to do it manually after code generation.
This problem is misleading, because segments 31-28 are located in ROM[0] register, 43-40 in ROM[1] register. Cube shows numbers 31-28, we try to write ROM[0] register, what is not working, because this segments has numbers 43-30 and we should write other register (ROM[1]). And this is because of wrong MUX_SEG bit settings.
Could you check this somehow?
2020-11-26 7:09 AM
Hello @KDwor.17
You need to check the check-box "multiplex mode" to obtain : hlcd.Init.MuxSegment = LCD_MUXSEGMENT_ENABLE .
Please use the latest CubeMX version.
Thanks
Khouloud
2023-09-24 1:15 AM
Thx a lot, this saved me a lot of time! I'm using a 1/4 duty cycle glass with 32 segments and used this as workaround:
for (int i = 0; i < 4; i++) {
HAL_LCD_Write(&hlcd, i * 2, 0, lcdram[i]);
HAL_LCD_Write(&hlcd, i * 2 + 1, 0, (lcdram[i] & 0xf0000000) >> 20);
}
HAL_LCD_UpdateDisplayRequest(&hlcd);I'm writing from my own shadow-registers the upper most 4 bits on the next register shifted by 20 bits, then it works with LCD_MUXSEGMENT_DISABLE.
But you are right, this is very confusing done.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.