2022-06-14 6:26 AM
I am using the example project GPIO_IOToggle_TrustZone for NUCLEO-U575ZI-Q and added Timer3 for Non-secure application via CubeMx with Interrupts enabled. When this Timer is started with HAL_TIM_Base_Start_IT the application runs into SecureFault_Handler.
Something seems to be not correctly configured by CubeMx.
2022-06-17 7:25 AM
Hi @Lukas Böhm ,
unfortnately the CubeMX cannot yet fully configure the Trustzone aspects by itself. I don't have the nucleo here with me, but I'll try to have a look next week.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.