2022-04-15 11:56 AM
When I attempt to create a task with a name longer than 15 characters, CubeMX seems to truncate to 15 characters max. How do I name a Task in CubeMX longer than 15 characcters?
Solved! Go to Solution.
2022-04-27 11:37 PM
Please change MAX_TASK_NAME_LEN (FreeRTOS 'Config parameters' tab) to desired length+1 (this +1 is for NULL at the end of the string). By default it is set to 16 this is why you can use max 15 characters within task name.
2022-04-27 11:37 PM
Please change MAX_TASK_NAME_LEN (FreeRTOS 'Config parameters' tab) to desired length+1 (this +1 is for NULL at the end of the string). By default it is set to 16 this is why you can use max 15 characters within task name.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.