2026-06-04 3:17 AM - last edited on 2026-06-04 4:52 AM by Andrew Neil
Hello Team,
We are developing a custom board based on the STM32N657 MCU. During pin assignment in the CubeMX tool, PB3 is shown with the JTDO_SWO function. However, the datasheet indicates that the SWO functionality is associated with PB5.
Could you please confirm which pin actually supports the SWO function?
Thanks
Solved! Go to Solution.
2026-06-04 4:58 AM
The User Manual for the NUCLEO-N657X0-Q (MB1940) shows SWO as PB5:
via: https://www.st.com/en/evaluation-tools/nucleo-n657x0-q.html#documentation
2026-06-04 4:24 AM - edited 2026-06-04 4:36 AM
If you click on PB5 will you see SWO there?
2026-06-04 4:57 AM - edited 2026-06-04 5:01 AM
Hi,
you did/have to choose in Cube :
..then the needed pins swd, sdc, swo are set/used for this.
On other cpu, here H743 :
But from ds it is PB5 on N657.
If wrong pin is set by Cube ...found a bug.
sidekick telling:
If you are seeing PB3 assigned as SWO in CubeMX, it may be a tool configuration issue or a recent update not reflected in the current documentation.
+
Are you using latest version/update of the tools ?
+
Gemini tells:
2026-06-04 4:58 AM
The User Manual for the NUCLEO-N657X0-Q (MB1940) shows SWO as PB5:
via: https://www.st.com/en/evaluation-tools/nucleo-n657x0-q.html#documentation
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.