2024-04-15 1:30 PM
Hello, I have a very simple code written with earlier versions of CubeIDE and FW_F4_1.26.2 for STM32F405rgt6
It is a very simple code, just sending a message via USB as a CDC Device . If I download the old .elf file to controller, everything works fine, but windows won't see the device nor get the messages when I compile it with 1.28.0 FW .
Is there a difference with usage? Or is there a bug with this?
Here is the code.
Solved! Go to Solution.
2024-04-24 4:19 AM
Hello @RÖztü.1 ,
First let me thank you for posting and welcome to the ST Community.
I suggest that you take a look at this Post.
The issue has been already reported internally to Dev team for correction (under internal ticket number 177153) and this will be fixed ASAP.
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-24 4:19 AM
Hello @RÖztü.1 ,
First let me thank you for posting and welcome to the ST Community.
I suggest that you take a look at this Post.
The issue has been already reported internally to Dev team for correction (under internal ticket number 177153) and this will be fixed ASAP.
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-17 11:33 AM
Thank you for information and also sorry for this very late answer.
Since there is still no fw update on f4 package, I wonder if there is a patch around? Or any workaround about this matter? I'm not able to create new projects with f4 chips using usb cdc while this problem going on.
Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.