STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

LevelX Setup for MX25R6435 on B-L4S5I-IOT01A

Attempting to create a project to access the onboard QuadSPI NOR flash (MX25R6435) on the SM32L4S5 Discovery kit. In STM32CubeMX, select the MX25R6435 under QuadSPI HAL says there is no QuadSPI HAL flash driver available, even though the stm32l4xx_ha...

SLimi.1 by Associate III
  • 2270 Views
  • 1 replies
  • 0 kudos

ST generated code warning

Hello,Getting a lot of these warnings in the ST generated code - prefer to be warning free, so legitimate, application code warnings are more obvious. I don't see the ability to suppress individual occurrences, and don't want to remove -Wregister com...

R_DSP_0-1716244187560.png
R_DSP by Associate II
  • 2274 Views
  • 3 replies
  • 1 kudos

Generate peripheral initialization to specific directory

STM32CubeIDE 1.10.1STM32CubeMX 6.6.1-RC2 In CubeMX -> Project Manager -> Code Generation there is an option to generate separate file pairs for the peripherals. These files are generated in the Core\Inc and Core\Src folder. Is there a way to have the...

gb2835 by Associate II
  • 1479 Views
  • 1 replies
  • 1 kudos

X-NUCLEO-GFX02Z1 with Nucleo-H755ZI-Q X-Cube Display Package

In the X-Cube Display Package there is a HelloWorld Application for X-NUCLEO-GFX02Z1 with a NUCLEO-H723ZG. Is it possible to change it in a way to make it on Nucleo-H755ZI-Q running?Otherwise, is there a step by step manual to get the display X-NUCLE...

guc by Associate II
  • 4990 Views
  • 8 replies
  • 0 kudos

My own Visual "Configurator"

Hi guys!Still live and kicking, thanks God! My fist public version was/is vscode_nucelo_l152re (totally uninspired, I am bad with naming things) that is a visual configuration tool for the Nucleo_L152RE board and generates code that uses the old SPL ...

Resolved! Did CubeMX 6.7 break H7 Clock Configuration?

Hi,I have just updated to CubeMx 6.7 and now my stm32H755 nucleo board shows error while setting to 480MHz. I'm pretty sure that this board can run this fast before.Did the new CubeMx break clock config feature for H7 devices? There is also this craz...

0693W00000WJnaxQAD.png 0693W00000WJnbgQAD.png
HHuyn.15 by Associate II
  • 4513 Views
  • 4 replies
  • 0 kudos

Resolved! CubeIDe 1.15.0 FW_f4_1.28.0 USB CDC not working

Hello, I have a very simple code written with earlier versions of CubeIDE and FW_F4_1.26.2 for STM32F405rgt6It is a very simple code, just sending a message via USB as a CDC Device . If I download the old .elf file to controller, everything works fin...

RÖztü.1 by Associate II
  • 3652 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.