2025-04-15 10:34 PM
Hello everyone,
I wanted to check if there is any updated information regarding when STM32CubeMX will officially enable generation and support of C++ code. Currently, I'm still relying on various workarounds to implement projects in C++, which unnecessarily complicates the development process.
Does anyone have new insights or know of an official roadmap from STMicroelectronics?
Adding native C++ support would be a significant improvement, especially for higher performance STM32 microcontrollers like the STM32H7, STM32U5, etc. series. C++ enables better code organization through object-oriented programming, making it easier to manage complex projects.
2025-04-16 12:37 AM
Hello @EniRot99
STM32CubeIDE can help generate C++ projects. You can follow these steps to convert a CubeMX project to a C++ project:
1-Generate the CubeMX project.
2- Open the project STM32CubeIDE
3- Right click on the project --> Convert to C++ Project" option to add C++ nature to the project.
4- Rename "main.c" to "main.cpp".
5- Adjust the project properties to use the C++ compiler and set the desired C++ standard
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-16 4:21 AM
yes this is a workaround I already did. The problem is, when you have to change a setting in CubeMX or expand the application, for example, adding a new peripheral CubeMX will overwrite your "main.cpp" with a newly generated "main.c". This makes the workflow tedious, as you constantly have to re-merge your previous C++ adaptations back into the project.
What we're really looking for is native C++ support directly in CubeMX. Ideally, CubeMX should directly generate ".cpp" files, so we don't have to manually adjust the code after every regeneration.
2025-04-16 4:35 AM
There is another, simpler, cleaner way, it has been discussed in this forum ad nauseum.
It is that you simply convert the project generated by Cube to C++. Then you simply develop your object oriented application in C++, and let the Cube do its business as usual.
Young C++ developers are invited to review their C++ classes and refresh on the extern "C" construct. No need to rename anything. That's all. It works.
2025-04-16 5:37 AM
Keep it as main.c and put your C++ code in another file. This is how it is meant to be done and avoids the annoyances you mention.
CubeMX is created to generate C code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.