cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX won't restart (won't turn on after shutdown)

STxuetu
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions

Hello @STxuetu 

Could you please try to delete \.stm32cubemx folder and check! 

Otherwise, could you check if some antivirus/firewall is activated?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Souhaib MAZHOUD
ST Employee

Hello @STxuetu 

Could you provide further information on the CubeMX version and OS you are using?

BR,

Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

STxuetu
Associate II

 i7-12700H 2.30 GHz,64-bit operating system, x64-based processor

STM32CubeMX-6.14.1

STxuetu
Associate II

After the first installation, you can open it once, close it and it will not open

i7-12700H 2.30 GHz,64-bit operating system, x64-based processor STM32CubeMX-6.14.1After the first installation, you can open it once, close it and it will not open

Hello @STxuetu 

Could you please try to delete \.stm32cubemx folder and check! 

Otherwise, could you check if some antivirus/firewall is activated?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi, I followed your instructions and deleted the \.stm32cubemx folder and was able to open cubemx successfully.

I'd like to ask if the deleted folder is redundant, I'd appreciate your guidance on this

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.