2016-08-10 2:08 AM
Hi to all, i use cubeMX and stm32F401re, all work weel but tree days ago i update the libraries for STM32F4 family, lather this update i create a simple project with cubemx,
when i compile whit IAR i have this error : Error[Ta097]: Cannot call intrinsic function ''__nounwind __DSB'' from Thumb mode in this architecture C:\MRC\example\Drivers\CMSIS\Include\core_cm4.h 1792 Error[Ta097]: Cannot call intrinsic function ''__nounwind __DSB'' from Thumb mode in this architecture C:\MRC\exemple\Drivers\CMSIS\Include\core_cm4.h 1797 Error while running C/C++ Compiler if i use KEIL all work well, can you help me? best regards Antonio #cubemx #!bug #iar2016-08-10 3:05 AM
Hi AntonioB,
If you are using an IAR version older than 7.50, please try to switch to a more recent one (>= 7.60).-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-08-22 2:05 AM
Hi Mayla, thanks for all, now all work well.
bye AntonioWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.