STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Generated uVision Project File is corrupted

When generating code in CubeMX for the MDK-ARM Toolchain, the uVision Project file (.uvprojx) is corrupted.When I try to open the project it shows the following message: Comparing the project files shows that the following section gets removed:Manual...

uvision.png diff.png
Jonas3 by Associate II
  • 1451 Views
  • 2 replies
  • 0 kudos

Several issues in CubeMx for STM32U0x3

For a project I am using the STM32U073 and for testing the development board with the STM32U083. I have encountered several issues in CubeMX and perhaps also in the hardware: The code that CubeMX generates for the low power timer contains a typo. Lin...

wijnen by Associate II
  • 1232 Views
  • 1 replies
  • 0 kudos

CubeMX bug regarding LPUART1 DMA (MX_Device.h)

I use the STM32L496ZG. When generating the files using STM32CubeMX it also generates MX_Device.h which contains several defines. When using LPUART1 with DMA it also generates defines like:#define MX_LPUART_RX_DMA_DMA_Handle #define MX_LPUART_RX_DMA_I...

Reneb by Associate III
  • 2295 Views
  • 3 replies
  • 0 kudos

Resolved! ADC not triggering ISR after each EOC

Hello st forum,I'm currently working with STM32G0B1VCI6, I'm trying to configure the ADC1 channel but it is not working properly. I need to convert 11 channels (10 external and 1 internal channel) and I'm configuring the driver in such a way it can c...

JDaniel1_0-1741809693267.png
JDaniel1 by Associate II
  • 1407 Views
  • 2 replies
  • 1 kudos

Resolved! Different FreeRTOS in latest CubeMX?

Hi,I just updated CubeIDE/CubeMX, and after creating a new project, I began configuring the microcontroller. However, when I tried to install FreeRTOS, it didn’t seem to be available. In the older version of CubeMX, there was a FreeRTOS option under ...

Ricko_2-1741046826671.png Ricko_0-1741046681156.png Ricko_0-1741049461926.png
Ricko by Senior III
  • 3347 Views
  • 5 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.