2016-02-28 11:14 AM
It would be nice if you could move into a header the definition of GPIO_MODE, GPIO_MODE, ... GPIO_CR_CNF_ANALOG, GPIO_CR_MODE_INPUT, GPIO_CR_CNF_ANALOG, ...GPIO_CR_CNF_AF_OUTPUT_OD currently in stm32fNxx_hal_gpio.c
These definitions may be useful to automatically generate configuration functions with external tools. CubeMX does a great job if you've to configure pins once but HAL_GPIO_Init() may be not as efficient as it has to be if you've to switch GPIO configuration in the middle of an interrupt and assigning pin functions manually is so '90 and is terribly error prone. Having to cut&paste code from stm32fNxx_hal_gpio.c is annoying and error prone as well. thanks #hal. #cubemx #headers2016-02-29 6:35 AM
Hi borgonovo.ivan_sergi,
In the stm32fNxx_hal_gpio.c, the private constants are defined: they are the constants that will be used ONLY locally in the current .c file.In the header file, you will find the defines for the parameters that you will need in the initialization of your GPIO for example.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.