STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Any way to change processor in CUBE?

Posted on July 25, 2016 at 22:02We have spent weeks getting the CubeMX setup just right, and have decided that we need a processor that has more memory. I really don't want to start from scratch, the processor is almost identical except that it has ...

mattreed9 by Associate III
  • 2285 Views
  • 1 replies
  • 0 kudos

Resolved! CubeMX, missing device-setting in generated EWARM project

Posted on July 13, 2016 at 04:05Hi, I encountered following. When I set device type as ''ST STM32F401xE'' on EWARM, the project was build successfully. Is the device type should determined everytime? with,   STM32CubeMX Version 4.15.1   STM32Cube FW...

STM32CubeMX Flash Latency Greyed Out (RCC Configuration)

Posted on July 21, 2016 at 16:03I have a question on how to modify the Flash Latency under RCC Configuration. No matter what clock configuration I choose, this field is always greyed out. In some application, I had to modify myself the Flash Latency...

ekawahyu2 by Associate II
  • 2520 Views
  • 3 replies
  • 0 kudos

STM32F446RE CubeMX HAL-SPI Problem

Posted on July 06, 2016 at 15:41Hello, I habe a two problems with the SPI-communication between a Nucleo64 and a X-Nucleo-IHM01A1 => STM32F446RE to L6474. 1. The CubeMx 4.15 creates following code in the �void HAL_SPI_MspInit(SPI_HandleTypeDef* spiH...

Sven1 by Associate II
  • 1390 Views
  • 1 replies
  • 0 kudos

ADC DMA problem

Posted on July 08, 2016 at 20:06Hi,    I am generating a CubeMX project for a STM32L476 (on a Nucleo boared).  I'm using 3 ADCs, 2 and 3 with DMA.  When I try to start a conversion, I am getting aHAL_ADC_STATE_ERROR_INTERNALin the conversion complet...

How to put HAL ISR into SRAM?

Posted on July 04, 2016 at 07:53My current SRAM usage on STM32F042 is miniscule.  Since there doesn't appear to be a way to shut off parts of the SRAM for lower current usage (am I wrong?), the next best thing I can do to save power is to move frequ...

hmc by Associate III
  • 1024 Views
  • 3 replies
  • 0 kudos

STM32F4 Discovery HAL LIBRARY Bit's not defined

Posted on June 30, 2016 at 18:13Hello,      In STM32F4 Discovery using HAL Library, bits 'CAN_FLAG_FMP0' and 'CAN_FLAG_FF1' of RF0R register and RF1R register are not defined in the 'stm32f4xx_hal_can.h' file. I have found bits 'CAN_RF0R_FMP0' and '...

ninad911 by Associate III
  • 1425 Views
  • 2 replies
  • 0 kudos

Auto detect budrate serial

Posted on June 28, 2016 at 11:48Hello,I have a STM32L031K6 and I want some auomatiser my reception function is adding automatic detection of transmission speed (baud rate) how I can do. thank you very much

ibrahim by Associate II
  • 5304 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.