2016-07-06 6:41 AM
Hello,
I habe a two problems with the SPI-communication between a Nucleo64 and a X-Nucleo-IHM01A1 => STM32F446RE to L6474.
1. The CubeMx 4.15 creates following code in the �void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle)
�**SPI1 GPIO Configuration
PA5------> SPI1_SCK PA6------> SPI1_MISO PA7------> SPI1_MOSI */ GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF5_SPI1; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); �.} Why GPIO_PIN_6 (= MISO) is defined as an output? I think it should be an input!?(I tried this also with other F4xx, F3xx and F7xx => all the same. It's already shown in the
CubeMX->Configuration->SPI-Settings->GPIO-Settings
and can&sharpt be changed. Funny thing: Creating project for a STM32F103RBT6 => MISO is an input!!So I modified the void HAL_SPI_MspInit to:
GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLUP; // (also tried NOPULL)
GPIO_InitStruct.Alternate = GPIO_AF5_SPI1; // should be obsolent
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
With this Init and HAL_SPI_Transmit I can send bytes to the L6474 (Stepper Controller).
With my analyzer I can see, that the L6474 sends the correct response-bytes.
I try to read it with:
if(HAL_SPI_TransmitReceive(&hspi1, (uint8_t*)aTxBuffer, (uint8_t *)aRxBuffer, 1, 1000) != HAL_OK)
{ Error_Handler(); }
The aTxBuffer is loaded with 0x00 for clocking the SCK
�but the aRxBuffer is always empty.(0x00).
Where is the (my?) mistake?The input-hardware should be fine � I can read a signal if I define Pin6 as a simple GPIO-input.
Thanks for your ideas
Sven
#cubemx-stm32f446-hal_spi2016-07-14 3:37 AM
Hi Sven,
Please note that the GPIOs are not managed the same way for STM32F1 family and other ones.You can refer to the reference manual of each family to know the differences.If the pin is configured in AF mode, it will be driven by the peripheral depending on its usage. So, there is no need to configure MISO pin in input mode for example with STM32F4.If you have issues with your generated project and updates you made for it, I suggest you review one of the SPI examples available in the STM32Cube packages. Test the example, and if it is OK compare your code with the one of the example.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.